Bug Report: Minor errors in USB Host code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bug Report: Minor errors in USB Host code

1,278 Views
chrissolomon
Contributor III

Hi,

I'm reviewing the changes in MQX 4.1.0 and spotted a couple of minor errors in the USB host code - (actually I am using v4.8.4 of the GCC compiler and these come out as warnings):

usb_host_msd_bo.c Line 109 -

   USB_mem_zero(intf_ptr, sizeof(USB_MASS_CLASS_INTF_STRUCT_PTR));

Looks like this is a typo - the intp_ptr is a pointer to a USB_MASS_CLASS_INTF_STRUCT, so it looks like the intention was that the whole structure be zeroed, where as in reality only the first 4 bytes are being zeroed.

Same thing in usb_host_printer.c at Line 468

   USB_mem_zero (prt_intf,sizeof(PRINTER_INTERFACE_STRUCT_PTR));

I don't think these are going to cause any problems, but I figured if you are still using version 4.7 of the compiler you might not have see these, and they look like quick and easy fixes.

Thanks

Chris

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,068 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Chris:

Thank you for reporting this, this will be fixed in next release

Have a great day

Daniel

0 Kudos
Reply