Bug Report: Cortex-A5 PSP boot.S interrupt stack.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bug Report: Cortex-A5 PSP boot.S interrupt stack.

ソリューションへジャンプ
2,860件の閲覧回数
billpringlemeir
Contributor V

I think that we need to use 'R0' and not 'R1' as it is not set anywhere.  It probably doesn't matter much as interrupts should be disabled until the actual interrupt stack is setup latter.  This is line 143 of MQX4.0.2 and 139 of MQX-4.1 in boot.S.  Is this where I should report issues or is there some SPR system?  Am I allowed to show the code lines or does this violate the MQX license?

タグ(3)
0 件の賞賛
返信
1 解決策
2,531件の閲覧回数
billpringlemeir
Contributor V
diff --git a/mqx/source/psp/cortex_a/core/A5/boot.S b/mqx/source/psp/cortex_a/core/A5/boot.S
index 7ae8de3..f2b33f1 100644
--- a/mqx/source/psp/cortex_a/core/A5/boot.S
+++ b/mqx/source/psp/cortex_a/core/A5/boot.S
@@ -131,12 +131,12 @@ ASM_LABEL(reset)
 
                 /* set fast interrupt (FIQ) mode stack */
                 msr cpsr_c, #PSP_PSR_MODE_FIQ | PSP_PSR_CTRL_DIS_FIQ | PSP_PSR_CTRL_DIS_IRQ
                 ldr sp, =FIQ_STACK_ADDR
 
                 /* set interrupt (IRQ) mode stack */
                 msr cpsr_c, #PSP_PSR_MODE_IRQ | PSP_PSR_CTRL_DIS_FIQ | PSP_PSR_CTRL_DIS_IRQ
                 ldr r0, =__BOOT_STACK_ADDRESS
-                mov sp, r1
+                mov sp, r0
 
                 /* set abort mode stack */
                 msr cpsr_c, #PSP_PSR_MODE_ABORT | PSP_PSR_CTRL_DIS_FIQ | PSP_PSR_CTRL_DIS_IRQ
                 msr cpsr_c, #PSP_PSR_MODE_ABORT | PSP_PSR_CTRL_DIS_FIQ | PSP_PSR_CTRL_DIS_IRQ

Later, the value 'r1' is updated, but at this point in the code, the value is random from reset.  There is also some commented code before that was attempting to set 'r1', but it is not active in MQX-4.1.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,531件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi Bill,

You can share the correction here, there is no issue or problem about it.

Best Regards,

Alejandro

0 件の賞賛
返信
2,532件の閲覧回数
billpringlemeir
Contributor V
diff --git a/mqx/source/psp/cortex_a/core/A5/boot.S b/mqx/source/psp/cortex_a/core/A5/boot.S
index 7ae8de3..f2b33f1 100644
--- a/mqx/source/psp/cortex_a/core/A5/boot.S
+++ b/mqx/source/psp/cortex_a/core/A5/boot.S
@@ -131,12 +131,12 @@ ASM_LABEL(reset)
 
                 /* set fast interrupt (FIQ) mode stack */
                 msr cpsr_c, #PSP_PSR_MODE_FIQ | PSP_PSR_CTRL_DIS_FIQ | PSP_PSR_CTRL_DIS_IRQ
                 ldr sp, =FIQ_STACK_ADDR
 
                 /* set interrupt (IRQ) mode stack */
                 msr cpsr_c, #PSP_PSR_MODE_IRQ | PSP_PSR_CTRL_DIS_FIQ | PSP_PSR_CTRL_DIS_IRQ
                 ldr r0, =__BOOT_STACK_ADDRESS
-                mov sp, r1
+                mov sp, r0
 
                 /* set abort mode stack */
                 msr cpsr_c, #PSP_PSR_MODE_ABORT | PSP_PSR_CTRL_DIS_FIQ | PSP_PSR_CTRL_DIS_IRQ
                 msr cpsr_c, #PSP_PSR_MODE_ABORT | PSP_PSR_CTRL_DIS_FIQ | PSP_PSR_CTRL_DIS_IRQ

Later, the value 'r1' is updated, but at this point in the code, the value is random from reset.  There is also some commented code before that was attempting to set 'r1', but it is not active in MQX-4.1.

0 件の賞賛
返信
2,531件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Thanks a lot Bill!!

Best Regards,

Alejandro