Bootloader example code for MQX 4.2 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bootloader example code for MQX 4.2 ?

Jump to solution
5,575 Views
王志升
Contributor I

Hello,

I am porting my system from MQX 4.0 to MQX 4.2  but I can't find example code of "Bootloader" in version 4.2.

I read the release note of MQX 4.2. It shows that Bootloader is avalable , but there is no example code.(there are only

bootloader_vybrid and bootloader_vybrid_qspixip.No bootloader!!)

I installed MQX4.1 before and I can see all the three item, but my system need MQX4.2 to support K64.

Or it's just no example, MQX 4.2. still support the old Bootloader of 4.0 & 4.1.

Thanks in advance.

Justin

1 Solution
5,288 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Justin:    

       

Unfortunately there isn't an example like what you need. The bootloader in MQX 4.1 is for Coldfire not for Kinetis devices.

However NXP/Freescale provides some application notes about Kinetis K product bootloader.  You can use this for reference.

AN4370 USB DFU Bootloader for MCUs 

http://cache.nxp.com/docs/en/application-note/AN4370.pdf?fsrch=1&sr=2&pageNum=1 

AN4368 USB MSD storage device host bootloader

http://cache.nxp.com/docs/en/application-note/AN4368.pdf?fsrch=1&sr=1&pageNum=1 

AN4379 Freescale USB Mass Storage Device bootloader

http://cache.nxp.com/docs/en/application-note/AN4379.pdf?fsrch=1&sr=1&pageNum=1 

AN4367 Ethernet Bootloader for MCU

http://cache.nxp.com/docs/en/application-note/AN4367.pdf?fsrch=1&sr=1&pageNum=1 

I hope it helps

Regards

Daniel

-------------------------------------------------------------------------------------

Note: Please click helpful or correct answer if it helps, thanks

View solution in original post

4 Replies
5,288 Views
王志升
Contributor I

Who has the experience of "TFTP Bootloader" on MQX4.2?

Please give me help.

      Justin

0 Kudos
Reply
5,289 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Justin:    

       

Unfortunately there isn't an example like what you need. The bootloader in MQX 4.1 is for Coldfire not for Kinetis devices.

However NXP/Freescale provides some application notes about Kinetis K product bootloader.  You can use this for reference.

AN4370 USB DFU Bootloader for MCUs 

http://cache.nxp.com/docs/en/application-note/AN4370.pdf?fsrch=1&sr=2&pageNum=1 

AN4368 USB MSD storage device host bootloader

http://cache.nxp.com/docs/en/application-note/AN4368.pdf?fsrch=1&sr=1&pageNum=1 

AN4379 Freescale USB Mass Storage Device bootloader

http://cache.nxp.com/docs/en/application-note/AN4379.pdf?fsrch=1&sr=1&pageNum=1 

AN4367 Ethernet Bootloader for MCU

http://cache.nxp.com/docs/en/application-note/AN4367.pdf?fsrch=1&sr=1&pageNum=1 

I hope it helps

Regards

Daniel

-------------------------------------------------------------------------------------

Note: Please click helpful or correct answer if it helps, thanks

5,019 Views
jjt
Contributor I

The app note might help, but the link you provide returns "Not Found". 

AN4367 Ethernet Bootloader for MCU

http://cache.nxp.com/docs/en/application-note/AN4367.pdf?fsrch=1&sr=1&pageNum=1 

 

 

0 Kudos
Reply
5,054 Views
jjt
Contributor I

Link for AN4367 no longer links to anything.

Search for AN4367 is also a dead end.

Is there any support for a K60 ethernet based boot loader?

0 Kudos
Reply