Are two partition manager for two primary partitions needed or not?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Are two partition manager for two primary partitions needed or not?

跳至解决方案
1,485 次查看
Fabi
Contributor III

Hi community,

for the partition manager I need some clarification. I've two primary partitions onto one SD card. To access both partitions, I've to setup two partition manager.  Here's the code snipped that works:

// Install partition manager over SD card driver, acquire full disk space

result = _io_part_mgr_install ( hdCard, "pm:", 0 );

         // error handling omitted here...

// Open partition manager

hdCardPart1 = fopen ( "pm:", NULL );

         // error handling omitted here...

// Validate partition 1

param = 1;

result = _io_ioctl ( hdCardPart1, IO_IOCTL_VAL_PART, &param );

if ( result == MQX_OK )

{

    // Install MFS over partition 1

    result = _io_mfs_install ( hdCardPart1, "c:", param );

             // error handling omitted here...

}

// Open file system

hd_1 = fopen ( "c:", NULL );

result = ferror ( hd_1 );

         // error handling omitted here...

// Open partition manager

hdCardPart2 = fopen ( "pm:", NULL );

         // error handling omitted here...

// Validate partition 2

param = 2;

result = _io_ioctl ( hdCardPart2, IO_IOCTL_VAL_PART, &param );

if ( result == MQX_OK )

{

    // Install MFS over partition 2

    result = _io_mfs_install ( hdCardPart2, "d:", param );

             // error handling omitted here...

}

hd_2 = fopen ( "d:", NULL );

result = ferror ( hd_2 );

         // error handling omitted here...

My question is, why two partition managers (hdCardPart1 and hdCardPart2) are needed?

That is to say, the following code snipped doesn't work:

// some code omitted here...

result = _io_mfs_install ( hdCardPart1, "c:", param );

// some code omitted here...

result = _io_mfs_install ( hdCardPart1, "d:", param ); // re-use the first partition manager for second partition -> not working

I use MQX 4.0.2.2 on MK60DN512.

TY

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,182 次查看
RadekS
NXP Employee
NXP Employee

It is that way, because this is correct way.

You can have file system

  1. directly on disk
  2. indirectly on partition.

In second case, file system has to be installed on partition and file system doesn’t care what is below partition. Parameter partition_num will be removed in next MFS version (released probably in MQX 4.2 package).


Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,183 次查看
RadekS
NXP Employee
NXP Employee

It is that way, because this is correct way.

You can have file system

  1. directly on disk
  2. indirectly on partition.

In second case, file system has to be installed on partition and file system doesn’t care what is below partition. Parameter partition_num will be removed in next MFS version (released probably in MQX 4.2 package).


Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,182 次查看
Fabi
Contributor III

Fine. Would it be better to distinguish the string identifier? In other words, should

hdCardPart1 = fopen ( "pm1:", NULL );

hdCardPart2 = fopen ( "pm2:", NULL );

be used instead of

hdCardPart1 = fopen ( "pm:", NULL );

hdCardPart2 = fopen ( "pm:", NULL );

or doesn't matter?

0 项奖励
回复
1,182 次查看
RadekS
NXP Employee
NXP Employee

In fact, you have two correct options how to select appropriate partition:

  1. Select partition by string identifier
  2. Select partition subsequently by ioctl command

a)

// Install partition manager over SD card driver, acquire full disk space

result = _io_part_mgr_install ( hdCard, "pm:", 0 );

hdCardPart1 = fopen ( "pm:1", NULL );

hdCardPart2 = fopen ( "pm:2", NULL );

//pm:0 is whole device; pm:1, pm:2, pm:3, pm:4 are partitions

b)

// Install partition manager over SD card driver, acquire full disk space

result = _io_part_mgr_install ( hdCard, "pm:", 0 );

hdCardPart1 = fopen ( "pm:", NULL );

partition_number = 1;

error_code = ioctl(hdCardPart1, IO_IOCTL_SEL_PART, &partition_number);

hdCardPart2 = fopen ( "pm:", NULL );

partition_number = 2;

error_code = ioctl(hdCardPart2, IO_IOCTL_SEL_PART, &partition_number);

// partition_number=0 is whole device, 1, 2, 3, 4 are partitions

I hope it helps you.

0 项奖励
回复