ARM MDK Keil uVision Support – Optimization in Release target MQX libraries

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ARM MDK Keil uVision Support – Optimization in Release target MQX libraries

Jump to solution
3,017 Views
pmt
Contributor V

From the Dec 2011 MQX-uVision getting started guide:

 

6.20 ARM MDK Keil uVision Support – Optimization in Release target MQX libraries

The code optimization level in the ARM MDK Keil uVision Release target is reduced to 0. Sporadic application crashes were observed in case any higher optimization level was used. The root cause of the issue was not known at the release date.

 

This seems like a major issue.  Has this been resolved?  I contacted Keil but they know nothing about it.

 

1 Solution
2,615 Views
c0170
Senior Contributor III

This is duplicate thread, I am closing this one which is older. Here's an answer:

Sporadic application crashes when running Keil / MQX above Optimization 0

Regards,

MartinK

View solution in original post

2 Replies
2,615 Views
BryGuyH
Contributor IV
2,616 Views
c0170
Senior Contributor III

This is duplicate thread, I am closing this one which is older. Here's an answer:

Sporadic application crashes when running Keil / MQX above Optimization 0

Regards,

MartinK