ARM MDK Keil uVision Support – Optimization in Release target MQX libraries

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ARM MDK Keil uVision Support – Optimization in Release target MQX libraries

ソリューションへジャンプ
3,019件の閲覧回数
pmt
Contributor V

From the Dec 2011 MQX-uVision getting started guide:

 

6.20 ARM MDK Keil uVision Support – Optimization in Release target MQX libraries

The code optimization level in the ARM MDK Keil uVision Release target is reduced to 0. Sporadic application crashes were observed in case any higher optimization level was used. The root cause of the issue was not known at the release date.

 

This seems like a major issue.  Has this been resolved?  I contacted Keil but they know nothing about it.

 

1 解決策
2,617件の閲覧回数
c0170
Senior Contributor III

This is duplicate thread, I am closing this one which is older. Here's an answer:

Sporadic application crashes when running Keil / MQX above Optimization 0

Regards,

MartinK

元の投稿で解決策を見る

2 返答(返信)
2,617件の閲覧回数
BryGuyH
Contributor IV
2,618件の閲覧回数
c0170
Senior Contributor III

This is duplicate thread, I am closing this one which is older. Here's an answer:

Sporadic application crashes when running Keil / MQX above Optimization 0

Regards,

MartinK