ARM MDK Keil uVision Support – Optimization in Release target MQX libraries

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ARM MDK Keil uVision Support – Optimization in Release target MQX libraries

跳至解决方案
2,178 次查看
pmt
Contributor V

From the Dec 2011 MQX-uVision getting started guide:

 

6.20 ARM MDK Keil uVision Support – Optimization in Release target MQX libraries

The code optimization level in the ARM MDK Keil uVision Release target is reduced to 0. Sporadic application crashes were observed in case any higher optimization level was used. The root cause of the issue was not known at the release date.

 

This seems like a major issue.  Has this been resolved?  I contacted Keil but they know nothing about it.

 

1 解答
1,776 次查看
c0170
Senior Contributor III

This is duplicate thread, I am closing this one which is older. Here's an answer:

Sporadic application crashes when running Keil / MQX above Optimization 0

Regards,

MartinK

在原帖中查看解决方案

2 回复数
1,776 次查看
BryGuyH
Contributor IV
1,777 次查看
c0170
Senior Contributor III

This is duplicate thread, I am closing this one which is older. Here's an answer:

Sporadic application crashes when running Keil / MQX above Optimization 0

Regards,

MartinK