ADC interrupt problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC interrupt problem

Jump to solution
4,032 Views
vitormayer
Contributor II

I am using MQX lite 1.1.1 and when I try to use ADC_LDD with interrupt i got the message:
Description Resource Path Location Type
undefined reference to `AD1_OnMeasurementComplete' AD1.c /my_project/Generated_Code line 399 C/C++ Problem

If I try use another timer interrupt, and I got the same message.

I  had all #include declared.


Any one could help me?

0 Kudos
Reply
1 Solution
3,933 Views
vitormayer
Contributor II

I am using KDS3.0.0 with a custom board with processor Mk64f.

Thank you for your attention, But I find the problem.

It was when I generate the PEx code, the new part of code was created inside the another function, and it was generating the undefine reference.

thanks one more time.

View solution in original post

0 Kudos
Reply
2 Replies
3,934 Views
vitormayer
Contributor II

I am using KDS3.0.0 with a custom board with processor Mk64f.

Thank you for your attention, But I find the problem.

It was when I generate the PEx code, the new part of code was created inside the another function, and it was generating the undefine reference.

thanks one more time.

0 Kudos
Reply
3,933 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Vitor:

Could you please provide more information for us to reproduce your issue? Which IDE you are using. Codewarrior 10.7 or KDS 3.2?   TWR-K64 board or other?

Regards

Daniel

0 Kudos
Reply