52259 auto negotiation problem?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

52259 auto negotiation problem?

3,721 Views
CarlFST60L
Senior Contributor II

Hi,

 

I think the 52259evb has auto negotiation problems with 1Gb switch's, is this a known issue, or is there a solution? I have found other products from freescale have similar problems.

 

I only have 2 x 1Gb switch's to test on, and both will not work. I dont know what else I can do from here. 

 

I have no problems on any 10/100Mb switchs I have tested on.

 

Carl.

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

1,813 Views
CarlFST60L
Senior Contributor II

Anyone?

 

Can someon comment 1Gb switchs should all work?

0 Kudos
Reply

1,813 Views
CarlFST60L
Senior Contributor II

I have just tested this on MQX3.5 and this is still a problem.

 

Anyone had a similar problem, or, do you know how to force it to work?

0 Kudos
Reply

1,813 Views
boogy
Contributor III

I have designed a board that uses the micrel KZ8873MLL (dual port switch) or the micrel KZ8041 (same as the M52259DEMO).

The KZ8041 works fine with a gigabit switch but the KZ8873MLL  does not. The problem is with the auto-negotiation.

I am new to MQX and I am having trouble finding out where the register's are set-up. I am using the KZ8041 files to drive the KZ8873MLL. How do I write to the registers through the M11 port? 

0 Kudos
Reply

1,813 Views
boogy
Contributor III

Problem solved!:smileyvery-happy:

The ISET resistor was the incorrect value for the chip. Once it was changed all is well.