z4 and z7 cores in the mpc 5775k processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

z4 and z7 cores in the mpc 5775k processor

4,281 Views
pingfang
Contributor III

Hello!

When using the MPC5775K processor, I have the following problems, please help with technical support:

(1) how do the Z4 and Z7 cores  work , and what are the specific processes?

(2) If Z4 and two Z7 cores are used together in one project, how do they distribute the functionality of these three cores?

In addition, please provide relevant program code, case and technical information.

Look forward to your reply, thank you!

Labels (1)
Tags (3)
6 Replies

3,614 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

please check the example below. It shows, how to use all cores including interrupts.

https://community.nxp.com/docs/DOC-329809 

If you have any other questions, please feel free to write me back.

Regards,

Martin

3,614 Views
pingfang
Contributor III

Thank you for your reply.

How do z4 and z7 core interact with each other?

Is there any code about the millimeter wave radar?

Look forward to your reply, thank you!

0 Kudos
Reply

3,614 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

each core works independently and there is no interaction by default. You can fro example share memory or another resources between the cores, please see example below.

https://community.nxp.com/docs/DOC-329941 https://community.nxp.com/docs/DOC-329941

About radar example, unfortunately there is no code available and there is also no free support for radar module.

Regards,

Martin

3,614 Views
pingfang
Contributor III

how  to download the radar SDK?

0 Kudos
Reply

3,614 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

please submit case via NXP support page and I will assign your case and contact my colleague, who will generate registration code, which you will use for SDK downloading.

https://community.nxp.com/docs/DOC-329745?sr=search&searchId=42935c2f-d7b7-4e9b-a293-19ce8e57986d&se... 

Regards,

Martin

3,614 Views
pingfang
Contributor III

Thank you very much. How to download radar SDK?

0 Kudos
Reply