some questions about Timed serial Bus(TSB) and Microsecond Channel downstream(MSC)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

some questions about Timed serial Bus(TSB) and Microsecond Channel downstream(MSC)

2,657件の閲覧回数
huayeshen
Contributor I

Hello  NXP Teams:

I am using MPC5777M,the DSPI has a mode called "Timed Serial Bus ",the document said it can be support in DSI, but i can not make clear how the TSB working in DSI.

  By the way,the  proper noun “ MicroSecond Channel (MSC) downstream” i don't uderstand too ,so what is the MicroSecond Channel (MSC) downstream ?is there any  references?

huayeshen_0-1691747905009.png

 

0 件の賞賛
返信
3 返答(返信)

2,628件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

“MicroSecond Channel (MSC) downstream” means just the transmit path from MCU (master) to the device (slave).

0 件の賞賛
返信

2,629件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

In the past I have tested DSPI serialization what’s already configuration similar to microsecond bus (on this device the feature is called timed serial bus TSB):

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5746R-DSPI-serialization-S32DS-Power-...

Microsecond bus protocol consist additional features to the SPI. These would be needed to configure and add to mentioned example and you will get MSC example:

1 ) serialization of internal timers

2) LVDS terminal pairs (positive and negative) for data output and clock

3) changes in data format

For SOUT and SCLK it is needed to choose and configure pins properly according excel sheet embedded to the device’s RM.

0 件の賞賛
返信

2,613件の閲覧回数
huayeshen
Contributor I
Thank you, so what is the meaning of TSB? It seems like just a simple way of communication between one host and multiple slaves
0 件の賞賛
返信