programming spec for SPC5741PK1AMLQ5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

programming spec for SPC5741PK1AMLQ5

1,538件の閲覧回数
jackhsu
Contributor III

Hi,

Recently we need to support SPC5741PK1AMLQ5 on our programmer system.

May i know where can find out the programming spec for SPC5741PK1AMLQ5?

Please let us know if we need to sign NDA. Thank you.

0 件の賞賛
返信
1 返信

1,481件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

 

I can recommend this application note written for MPC56xx devices:

https://www.nxp.com/docs/en/application-note/AN4365.pdf

 

There's no application note written directly for MPC57xx devices but the AN4365 is still usable because not much has changed. As the MPC574xP is a VLE instruction only device, please take care to utilize the VLE instructions detailed in AN4365.

 

This sample script could help – it follows AN4365:

https://community.nxp.com/docs/DOC-332727

 

Table 9 in AN4365 details which drivers should be used for the MPC56xx devices. Obviously this is different for the MPC574xP device, so you should use the same procedure but with this driver:

 

https://www.nxp.com/webapp/Download?colCode=C55_NVM_SSD

 

By the way, SSD drivers for MPC57xx use new asynchronous design, so it is a little bit different comparing to MPC56xx SSD drivers.

 

Regards,

Lukas

0 件の賞賛
返信