Example JTAG access – Addendum to application notes AN3283 and AN4365

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example JTAG access – Addendum to application notes AN3283 and AN4365

Example JTAG access – Addendum to application notes AN3283 and AN4365

This example follows application notes AN3283 and AN4365. It is intended for users who develop own JTAG programmer.

It shows how to implement basic functions:

- enter debug mode during reset

- enable external debug mode

- OnCE access to GPR, SPR and memory

- Nexus access to memory

The example is written in PRACTICE script language using Trace32 debugger from Lauterbach (www.lauterbach.com). Low level functions for JTAG are used, so users can see sequences of ‘0’s and ‘1’s which are sent to JTAG interface. Used commands are described in this document:

www2.lauterbach.com/pdf/general_ref_j.pdf

This example was tested on MPC5607B device and VLE instruction set was used for OnCE access.

Labels (1)
Attachments
100% helpful (1/1)
Version history
Last update:
‎09-23-2016 01:19 AM
Updated by: