flash programming for MPC5748G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flash programming for MPC5748G

2,783 Views
huqiang
Contributor IV

Hello,

Was it possible that I use the S32 design studio and PE to do flash programming for MPC5748G?

I know that Lauterbach T32 can be used to do this, but how about using the S32 desgin studio and PE?

I need to put a "x.elf" file to a specified memory address。

Best regards,

Hu

0 Kudos
Reply
3 Replies

2,358 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Yes, you can use S32DS with PE Micro. There is no issue and it is commonly used.

However for serious development I recommend Lauterbach.

Peter

0 Kudos
Reply

2,358 Views
huqiang
Contributor IV

Hello, 

Do you have any instruction about how to do this?

Where can I configure the specified memory address?

I only have the "x.elf" file instead of making a project and debugging in S32 DS.

How can I directly put "x.elf" file to a specified memory address.

 

Best regards,

Hu

0 Kudos
Reply

2,358 Views
stanish
NXP Employee
NXP Employee

Hi Hu,

Please see this document:

https://community.nxp.com/docs/DOC-332252 

Hope it helps.

Stan

0 Kudos
Reply