flash programming for MPC5748G

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

flash programming for MPC5748G

2,863件の閲覧回数
huqiang
Contributor IV

Hello,

Was it possible that I use the S32 design studio and PE to do flash programming for MPC5748G?

I know that Lauterbach T32 can be used to do this, but how about using the S32 desgin studio and PE?

I need to put a "x.elf" file to a specified memory address。

Best regards,

Hu

0 件の賞賛
返信
3 返答(返信)

2,438件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Yes, you can use S32DS with PE Micro. There is no issue and it is commonly used.

However for serious development I recommend Lauterbach.

Peter

0 件の賞賛
返信

2,438件の閲覧回数
huqiang
Contributor IV

Hello, 

Do you have any instruction about how to do this?

Where can I configure the specified memory address?

I only have the "x.elf" file instead of making a project and debugging in S32 DS.

How can I directly put "x.elf" file to a specified memory address.

 

Best regards,

Hu

0 件の賞賛
返信

2,438件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi Hu,

Please see this document:

https://community.nxp.com/docs/DOC-332252 

Hope it helps.

Stan

0 件の賞賛
返信