flash_example_mpc5746c Questions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

flash_example_mpc5746c Questions

ソリューションへジャンプ
1,431件の閲覧回数
kimdukyu
Contributor II

Hi.

 

The register information of MPC5746C Reference Manual and S32DS is different.

kimdukyu_0-1659351471592.png

kimdukyu_1-1659351486259.png

 

What represents the correct register information? What if I want to unlock the mid block of 0x00FA000?

Is it okay to input the value of 0x00000000U in the mid block like the example program? please answer about my question.

 

Thank you

 

0 件の賞賛
返信
1 解決策
1,425件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

the confusing part here is that S32DS debugger obviously uses different bit ordering. The reference manual marks LSB bit as bit number 31 while S32DS marks LSB bit as 0.

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,426件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

the confusing part here is that S32DS debugger obviously uses different bit ordering. The reference manual marks LSB bit as bit number 31 while S32DS marks LSB bit as 0.

Regards,

Lukas

0 件の賞賛
返信