flash erasing-reset escalation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

flash erasing-reset escalation

2,064件の閲覧回数
abdelrhman
Contributor III

MPC5744p is uploaded with a code causing the the board to enter a reset state escalation 

and the s32 can not detect the the board due to reset state escalation

how to erase that code ??

0 件の賞賛
返信
2 返答(返信)

1,902件の閲覧回数
Amr_Awny
Contributor II
0 件の賞賛
返信

2,058件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

You have to connect right after core leaves the reset and before the reset is triggered by micro.

For example Lauterbach debugger use "halt core on power on reset" script:

petervlna_0-1633951050397.png

Find out how you can stop code execution on your debugger.

You can also have a look at following thread (it is for MPC5748G but the resolve is the same for all reset escalation issues)

https://community.nxp.com/t5/MPC5xxx/MPC5748G-Cannot-attached-JTAG-after-erase-all/m-p/617380

 

Best regards,

Peter

0 件の賞賛
返信