flash erasing-reset escalation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flash erasing-reset escalation

2,085 Views
abdelrhman
Contributor III

MPC5744p is uploaded with a code causing the the board to enter a reset state escalation 

and the s32 can not detect the the board due to reset state escalation

how to erase that code ??

0 Kudos
Reply
2 Replies

1,923 Views
Amr_Awny
Contributor II
0 Kudos
Reply

2,079 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

You have to connect right after core leaves the reset and before the reset is triggered by micro.

For example Lauterbach debugger use "halt core on power on reset" script:

petervlna_0-1633951050397.png

Find out how you can stop code execution on your debugger.

You can also have a look at following thread (it is for MPC5748G but the resolve is the same for all reset escalation issues)

https://community.nxp.com/t5/MPC5xxx/MPC5748G-Cannot-attached-JTAG-after-erase-all/m-p/617380

 

Best regards,

Peter

0 Kudos
Reply