etpuc files

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

etpuc files

跳至解决方案
3,168 次查看
InhyeokHwang
Contributor III

Hello NXP team,

I am currently studying eTPU development referencing AN4907.

I am using Code Warrior for eTPU v10.3.

From AN4907SW, I can find etpuc_cam.c, etpuc_crank.c ... the eTPU functions that are listed on AN4907 but I have no idea where I can get other etpuc functions for PWM, Input capture, output compare and so on. (or do these functions unnecessary to create microcode?)

I am also curious about the compilation in the eTPU project.

According to the reference, the compilation of the etpuc files create microcode.

Is the microcode located at ETPU configuration > cpu > etpu_set.h  the right code generated from compilation?

thanks.

 

 

0 项奖励
回复
1 解答
3,134 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

I just created overview document, where you can find out where to find source codes for eTPU functions.

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Links-to-source-codes-for-eTPU-functions-May-202...

 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,029 次查看
DRcapri
Contributor I

If I uderstand correctly, the source code files are available per request?

0 项奖励
回复
3,015 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, if mentioned so, then you will need submit a ticket for it:

https://www.nxp.com/support/support:SUPPORTHOME

 

 

0 项奖励
回复
3,010 次查看
DRcapri
Contributor I

thank you for your help. Will do, after I am getting more familiar with the application.

0 项奖励
回复
3,135 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

I just created overview document, where you can find out where to find source codes for eTPU functions.

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Links-to-source-codes-for-eTPU-functions-May-202...

 

0 项奖励
回复