etpuc files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

etpuc files

Jump to solution
806 Views
InhyeokHwang
Contributor III

Hello NXP team,

I am currently studying eTPU development referencing AN4907.

I am using Code Warrior for eTPU v10.3.

From AN4907SW, I can find etpuc_cam.c, etpuc_crank.c ... the eTPU functions that are listed on AN4907 but I have no idea where I can get other etpuc functions for PWM, Input capture, output compare and so on. (or do these functions unnecessary to create microcode?)

I am also curious about the compilation in the eTPU project.

According to the reference, the compilation of the etpuc files create microcode.

Is the microcode located at ETPU configuration > cpu > etpu_set.h  the right code generated from compilation?

thanks.

 

 

0 Kudos
1 Solution
772 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I just created overview document, where you can find out where to find source codes for eTPU functions.

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Links-to-source-codes-for-eTPU-functions-May-202...

 

View solution in original post

0 Kudos
4 Replies
667 Views
DRcapri
Contributor I

If I uderstand correctly, the source code files are available per request?

0 Kudos
653 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, if mentioned so, then you will need submit a ticket for it:

https://www.nxp.com/support/support:SUPPORTHOME

 

 

0 Kudos
648 Views
DRcapri
Contributor I

thank you for your help. Will do, after I am getting more familiar with the application.

0 Kudos
773 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I just created overview document, where you can find out where to find source codes for eTPU functions.

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Links-to-source-codes-for-eTPU-functions-May-202...

 

0 Kudos