error in makefile

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

error in makefile

4,751件の閲覧回数
锦晖韩
Contributor II

i used the mpc5748g to test its enet using s32 DS.power.2017R1

there is a problempastedImage_1.png

how to sovle it?

ラベル(1)
タグ(3)
7 返答(返信)

4,364件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

I suppose you created project from SDK example, am I correct?

Could you please share more details or share the example?

Regards,

Martin

0 件の賞賛
返信

4,364件の閲覧回数
锦晖韩
Contributor II

pastedImage_1.png

0 件の賞賛
返信

4,364件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

from your description it looks like you are trying to mix two projects together. This is not good way. If you want to create project using SDK, I recommend you install S32 Design Studio 2017.R1 with the newest update

S32 Design Studio for Power Architecture 2017.R1 (Windows/Linux) released! 

S32 Design Studio for Power Architecture 2017.R1 - Update 1 available 

and use enet_ping_mpc5748g example code (enet driver example) or lwip_mpc5748g (whole application with TCP/IP stack).

Please see the figure below:

pastedImage_3.png

Regards,

Martin

4,364件の閲覧回数
锦晖韩
Contributor II

Hello

Could you help me about the problem i asked?

Regards,

Jinhui

0 件の賞賛
返信

4,363件の閲覧回数
锦晖韩
Contributor II

Hello,

I test the 'enet-ping-5748g' project you advised ,but there are still some problems. After the debug and run the project , I can't recieve the message the board sent. Could you help me to find the reason and fix it.(It seems that the register is full after the first sent) Thanks a lot.

Regards,

Jinhui

0 件の賞賛
返信

4,363件の閲覧回数
锦晖韩
Contributor II

Hello,

I want to make a project using SDK, so i made a project about ENET . The project showed always without SDK, when I add it to the project I made, there are lots of warnings. Could you help me about how to add the project the community showed to the project with SDK. (I want to use it because I want to use the pins which the SDK has already defined.)

Regards,

Jinhui

0 件の賞賛
返信

4,363件の閲覧回数
锦晖韩
Contributor II

pastedImage_1.png

0 件の賞賛
返信