Power Supply and Reset microcontroller from SBC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power Supply and Reset microcontroller from SBC

1,543 Views
raghurajappa
Contributor IV

My setup - KITFS6522LAEEVM (FS6500) SBC with the MPC5643L (mounted on the minimodule + motherboard). I have two questions that follow these images.
pastedImage_1.pngpastedImage_2.png

Questions
1. When I use the JTAG debugger to program the microcontroller, I can NOT provide a reset from the SBC to the microcontroller because the JTAG debugger holds the reset line. Is this understanding correct?? For now I am using the serial programming (SCI) using RappID bootloader. The question is more a clarification. 

2. I can program the microcontroller through the SCI when I use the standalone DC power supply of 12V but I cannot program the microcontroller through the SCI when I use the power supply from the SBC (3.3V). I notice the SCI line voltages are the SAME when I use the two different power supplies. Why can I not program through the SCI while using the power supply (3.3V) from the SBC as indicated in the image below?
pastedImage_4.png


Thank you.

0 Kudos
Reply
1 Reply

1,317 Views
raghurajappa
Contributor IV

dumitru-daniel.popa‌, could you also please help me with the question above? Thank you. 

0 Kudos
Reply