eTimer PWM Generation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eTimer PWM Generation

4,279件の閲覧回数
flofa
Contributor II

Hello

i am using the eTimer peripheral for generating a PWM signal.

I use the "variable frequency mode" with "OUTMODE = toogle OFLAG O/P using alternating compare reg" and i can generate a PWM signal with duty cyles 1% to 99%.

I do not know how to generate a duty cyle of 0% (output signal = low) and a duty cycle of 100% (output signal = high).

How to generate these signals in variable frequency mode?

Maybe i have to switch the "OUTMODE" to "software controlled mode"?

Best regards,

Florian

ラベル(1)
タグ(3)
0 件の賞賛
返信
4 返答(返信)

4,045件の閲覧回数
flofa
Contributor II

I resolved it the following way for the VARIBALE-FREQUENCY-PWM-Mode:

If (DC = 0% or 100%)

Then OUTMODE = Software Controlled, VAL = 0 or 1, FORCE = 1

Else (0% < DC < 100%)

Then OUTMODE = toogle OFLAG O/P using alternating compare reg, CMPLD1 = off time, CMPLD2 = on time

Best regards,

Florian

0 件の賞賛
返信

4,045件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I have discussed it with my colleague and the only way to implement it like you do.

Peter

0 件の賞賛
返信

4,045件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

actually this is the way i would use it.

However I can on Monday ask colleague who has deep knowledge on it if there is any other way.

Peter

0 件の賞賛
返信

2,990件の閲覧回数
archanab1
Contributor I

Hi all,

I want to generate pwm with complementary and phase shift functionality using etimer module.

is it possible to achieve this? how?

 

Thanks

Archana

0 件の賞賛
返信