Why is this UID value set to 0 in the example code?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why is this UID value set to 0 in the example code?

Jump to solution
1,638 Views
InhyeokHwang
Contributor III

Hi NXP teams

I saw that UID is a unique value for each microcontrollers and it's set on the manufacturing process.

But in the process of the loadkey in the cse example code (cse_keyconfig_mpc5777c), I can see that uid is defined with value 0. 

Why is this so?

uid.PNGuid.PNG

0 Kudos
Reply
1 Solution
1,628 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @InhyeokHwang 

this is called wildcard UID and it is given by SHE specification.

All keys can be initially loaded using wildcard UID 0. Each key (except RAM key) have WILDCARD attribute. If you set this bit while loading a key, it's not possible to use wildcard UID anymore for this key. If you keep it '0', wildcard UID can be used also for updates of that key.

Regards,

Lukas

View solution in original post

0 Kudos
Reply
1 Reply
1,629 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @InhyeokHwang 

this is called wildcard UID and it is given by SHE specification.

All keys can be initially loaded using wildcard UID 0. Each key (except RAM key) have WILDCARD attribute. If you set this bit while loading a key, it's not possible to use wildcard UID anymore for this key. If you keep it '0', wildcard UID can be used also for updates of that key.

Regards,

Lukas

0 Kudos
Reply