Why is this UID value set to 0 in the example code?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why is this UID value set to 0 in the example code?

ソリューションへジャンプ
1,682件の閲覧回数
InhyeokHwang
Contributor III

Hi NXP teams

I saw that UID is a unique value for each microcontrollers and it's set on the manufacturing process.

But in the process of the loadkey in the cse example code (cse_keyconfig_mpc5777c), I can see that uid is defined with value 0. 

Why is this so?

uid.PNG

 

0 件の賞賛
返信
1 解決策
1,672件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @InhyeokHwang 

this is called wildcard UID and it is given by SHE specification.

All keys can be initially loaded using wildcard UID 0. Each key (except RAM key) have WILDCARD attribute. If you set this bit while loading a key, it's not possible to use wildcard UID anymore for this key. If you keep it '0', wildcard UID can be used also for updates of that key.

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,673件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @InhyeokHwang 

this is called wildcard UID and it is given by SHE specification.

All keys can be initially loaded using wildcard UID 0. Each key (except RAM key) have WILDCARD attribute. If you set this bit while loading a key, it's not possible to use wildcard UID anymore for this key. If you keep it '0', wildcard UID can be used also for updates of that key.

Regards,

Lukas

0 件の賞賛
返信