Where is the compile option window in Freescale Codewarrior IDE version 5.9.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is the compile option window in Freescale Codewarrior IDE version 5.9.0

1,181件の閲覧回数
missioncha
Contributor I

Hello everyone. 

In the middle of time to make a compilation of my source code in freescale codewarrior IDE version 5.9.0, it is awkward when it comes to look for the window of compile option or assmbly option or linker option to put into. 

by nature, I am thought of "Project -> Property" in which compile option is able to to correct a compile option setting. however, ui interface is invisible for them

please let me find out it through freescale codewarrior IDE version 5.9.0

Thanks in advance

0 件の賞賛
返信
4 返答(返信)

1,054件の閲覧回数
missioncha
Contributor I

Thank you so much for your kind findings and I've got hinted for my next step.  

0 件の賞賛
返信

1,056件の閲覧回数
missioncha
Contributor I

Thank you for a guide

0 件の賞賛
返信

1,102件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi, I'm not sure if I understand your question correctly.

You can go and check the compiler/linker options by Alt+F7 (Edit -> "Target" Settings...) keys or by clicking project settings icon (see screenshot below). There is no option to go to project settings in Project menu.

stanish_1-1704929082913.png

stanish_0-1704929300998.png

 

Hope it helps.

Stan

0 件の賞賛
返信

1,149件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Yes, that may be just right. During the compilation is most probably the configuration locked.

@stanish can you comment here?

Best regards,

Peter

0 件の賞賛
返信