WKPU HW Channel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,182件の閲覧回数
travis_kuo
Contributor III

Hi ,

In S32DS example wkpu_interrupt, we saw STM (System Timer Module)is WKUP HW channel #1. I don't know where is this documented.

Also we know PA1 pin is WKPU HW chhanel #2 in IO_Signal_Description_and_Input_multiplexing_tables.xls. See below.

May I know if there is any doc which specifies all WKPU HW channel HW channel ( wakeup sources)?

Thanks

PA[1] 10000_0000GPIO[1]SIUL2
PA[1]  0000_0001E0UC_1_GEMIOS0
PA[1]  -WKPU[2]WKPU
PA[1]  -NMI[0]WKPU
PA[1] 5130000_0010E0UC_1_GEMIOS0
PA[1] 7030000_0001CAN3RXFlexCAN_3
0 件の賞賛
返信
1 解決策
2,811件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

which microcontroller you use?

For example for MPC5746C, you can check the figure below.

pastedImage_1.png

Regards,

Martin

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,812件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

which microcontroller you use?

For example for MPC5746C, you can check the figure below.

pastedImage_1.png

Regards,

Martin

0 件の賞賛
返信
2,811件の閲覧回数
travis_kuo
Contributor III

Thanks.

I am using MPC5748G. And I found similar picture in the MPC5748G RM.

Thank you

0 件の賞賛
返信