Hi ,
In S32DS example wkpu_interrupt, we saw STM (System Timer Module)is WKUP HW channel #1. I don't know where is this documented.
Also we know PA1 pin is WKPU HW chhanel #2 in IO_Signal_Description_and_Input_multiplexing_tables.xls. See below.
May I know if there is any doc which specifies all WKPU HW channel HW channel ( wakeup sources)?
Thanks
PA[1] | 1 | 0000_0000 | GPIO[1] | SIUL2 | |
PA[1] | 0000_0001 | E0UC_1_G | EMIOS0 | ||
PA[1] | - | WKPU[2] | WKPU | ||
PA[1] | - | NMI[0] | WKPU | ||
PA[1] | 513 | 0000_0010 | E0UC_1_G | EMIOS0 | |
PA[1] | 703 | 0000_0001 | CAN3RX | FlexCAN_3 |
Solved! Go to Solution.
Hello,
which microcontroller you use?
For example for MPC5746C, you can check the figure below.
Regards,
Martin
Hello,
which microcontroller you use?
For example for MPC5746C, you can check the figure below.
Regards,
Martin
Thanks.
I am using MPC5748G. And I found similar picture in the MPC5748G RM.
Thank you