Time base frequency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Time base frequency

1,819件の閲覧回数
shitalshitole
Contributor II

How to calculate Time base frequency in eTPU module for PWM signal generation in MCP5777c?Please explain with any example with detail calculation.

ラベル(1)
2 返答(返信)

1,679件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I will show you screenshot from GCT tool, event though you use it or not.

Time base frequency for PWM function can be chosen as Engine A/B, TCR1/2

pastedImage_4.png

These are derived from system clock by selected pre-dividers:

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

That's the time base for PWM function.

1,679件の閲覧回数
shitalshitole
Contributor II

Thanks David for your valuable reply .Actually I have to calculate time base frequency without using GCT tool .I am using S32 design studio IDE and MCP5777c MCU.If I have to generate 1 KHZ pwm signal with 40% duty cycle so what should be Timebase frequency?Please provide calculation also and what is max and min limit of time base frequency?

0 件の賞賛
返信