Time base frequency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Time base frequency

1,855 Views
shitalshitole
Contributor II

How to calculate Time base frequency in eTPU module for PWM signal generation in MCP5777c?Please explain with any example with detail calculation.

Labels (1)
2 Replies

1,715 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I will show you screenshot from GCT tool, event though you use it or not.

Time base frequency for PWM function can be chosen as Engine A/B, TCR1/2

pastedImage_4.png

These are derived from system clock by selected pre-dividers:

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

That's the time base for PWM function.

1,715 Views
shitalshitole
Contributor II

Thanks David for your valuable reply .Actually I have to calculate time base frequency without using GCT tool .I am using S32 design studio IDE and MCP5777c MCU.If I have to generate 1 KHZ pwm signal with 40% duty cycle so what should be Timebase frequency?Please provide calculation also and what is max and min limit of time base frequency?

0 Kudos
Reply