Signal Processing on MPC5674

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Signal Processing on MPC5674

ソリューションへジャンプ
3,492件の閲覧回数
dpastl
Contributor II

Hi There,

 

I'm investigating adding signal processing to our product to attempt to reduce time spent on calculations.  I've been reading around on the SPE2 module for the MPC5674F but I can't figure out where to start.  Are there any libraries available, or application notes, on how to start using the SPE2 module with C?  What I'm really curious is, do I need to add a special library or if not, what header do I include?

 

Thanks!

 

David

ラベル(1)
0 件の賞賛
返信
1 解決策
3,367件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it should work as SPE units is backward compatible.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,367件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Following two libraries could be useful for you. These package contain a software and descriptive documents.

MPC55xx SPE DSP Library 1:

http://www.nxp.com/files/microcontrollers/software/app_software/code_examples/MPC55xx_SPE_DSP_Librar...

MPC55xx SPE DSP Library 2:

http://www.nxp.com/files/microcontrollers/software/app_software/code_examples/MPC55xx_SPE_DSP_Librar...

Also pay attention to following appnote

Improving DSP Performance Using Efficient SPE Coding (including FIR example):

http://www.nxp.com/files/microcontrollers/doc/app_note/AN3733.pdf

0 件の賞賛
返信
3,367件の閲覧回数
dpastl
Contributor II

Will the MPC55xx libraries work for a 56xx processor?

0 件の賞賛
返信
3,368件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it should work as SPE units is backward compatible.

0 件の賞賛
返信