Shadow Flash programming and NVUSRO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Shadow Flash programming and NVUSRO

ソリューションへジャンプ
2,871件の閲覧回数
fscheidl
Contributor II

I want to use an MPC5602D with a supply voltage of 5V. I read that I should program this in the NVUSRO[PAD3V5V] register in the shadow flash of the device in order for it to comply with the specified electrical characteristics - but it should work either way, right?

 

Now I am relatively new to Freescale products. Can I program the shadow flash via the Boot Assist Module only? (I am using this to program the MCU) If yes, is there any tutorial/example code for that? If no, what else do I need?

 

Thank you in advance!

ラベル(1)
タグ(3)
1 解決策
2,303件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

The PAD3V5V pin determines the slew rate for output drive pads to keep the rise time the same for a 3V configuration and 5V configuration. Yes, it is work in both cases, it is not dangerous anyhow to have it set in opposite configuration.

Shadow flash programming may be potentially dangerous because there is also censorship information there. Censorship feature is a way to prevent unauthorized access to the device. However it is very sensitive thing. It is needed to use it very carefully, because an inappropriate usage can lead in making the device useless. If user accidentally erases shadow flash/row there is no chance to recover it (unless it had been though about before).

In other aspects shadow flash is normal flash memory and may be programmed common ways. Example you may find here:

https://community.freescale.com/docs/DOC-102582

I would strongly recommend to read mentioned appnote.

元の投稿で解決策を見る

1 返信
2,304件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

The PAD3V5V pin determines the slew rate for output drive pads to keep the rise time the same for a 3V configuration and 5V configuration. Yes, it is work in both cases, it is not dangerous anyhow to have it set in opposite configuration.

Shadow flash programming may be potentially dangerous because there is also censorship information there. Censorship feature is a way to prevent unauthorized access to the device. However it is very sensitive thing. It is needed to use it very carefully, because an inappropriate usage can lead in making the device useless. If user accidentally erases shadow flash/row there is no chance to recover it (unless it had been though about before).

In other aspects shadow flash is normal flash memory and may be programmed common ways. Example you may find here:

https://community.freescale.com/docs/DOC-102582

I would strongly recommend to read mentioned appnote.