Shadow Flash direct programming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Shadow Flash direct programming

1,961 Views
jeffcampbell
Contributor III

Quick question - I'm attempting to alter shadow flash (fully aware of the risks; I've successfully done it already and am experimenting with the process).  Is it possible to edit the shadow block directly during the process of programming the chip (i.e. have a defined data section that gets loaded directly to Shadow Block A alongside the rest of the main program), or can it only be modified by a function executing from RAM?

Labels (1)
0 Kudos
Reply
1 Reply

1,827 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it is possible, if particular programmer have defined programming algorithm for shadow flash (for instance PeMicro debugger have them prepared …\pemicro\algorithms\shadow\).

Production programmers should be capable to do it as well as it can be just a requirement to set up censorship during production programming.

0 Kudos
Reply