Invalid OSR while core running (0x11F)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Invalid OSR while core running (0x11F)

1,712 Views
manuelsaez
Contributor II

Hello,

I am trying to get some traces to make code coverage with a PowerTrace II and a MPC5784G. When a let the program run I get the error message:

emulation debug port fail

error: received invalid OSR while core running (0x11F)

 

I have seen in the forum other people that gets the error code 0x000 and it is related to the reset. In this case the program should not being reset.

 

For the traces I tried the Incremental and SPY modes. BTM and HTM are activated.

 

What could be the problem? How can I investigate the source of the error?

 

Best regards,

Manuel

Labels (1)
0 Kudos
Reply
0 Replies