Sample LIN protocol code for MPC5777M .

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Sample LIN protocol code for MPC5777M .

3,394 次查看
anishchoudhary
Contributor III

I am working on MPC5777M EVB board and I want to develop LIN Protocol application on that board so any sample code of LIN is available or not in community ? and suggest me for useful document

标记 (1)
3 回复数

2,399 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you can refer to MPC5744P example posted here; https://community.nxp.com/docs/DOC-329922 

Teh LINFlex module is the same.

BR, Petr

2,399 次查看
anishchoudhary
Contributor III

Hi,

In the case of loop back test mode of LIN, external 12V is required or not.

BR, Anish

0 项奖励
回复

2,399 次查看
PetrS
NXP TechSupport
NXP TechSupport

I assume for internal loopback the transceiver is not used, so it is not needed to supply it.

BR, Petr