Sample LIN protocol code for MPC5777M .

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sample LIN protocol code for MPC5777M .

3,332件の閲覧回数
anishchoudhary
Contributor III

I am working on MPC5777M EVB board and I want to develop LIN Protocol application on that board so any sample code of LIN is available or not in community ? and suggest me for useful document

タグ(1)
3 返答(返信)

2,337件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you can refer to MPC5744P example posted here; https://community.nxp.com/docs/DOC-329922 

Teh LINFlex module is the same.

BR, Petr

2,337件の閲覧回数
anishchoudhary
Contributor III

Hi,

In the case of loop back test mode of LIN, external 12V is required or not.

BR, Anish

0 件の賞賛
返信

2,337件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

I assume for internal loopback the transceiver is not used, so it is not needed to supply it.

BR, Petr