SPC5748G flexlin LIN example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPC5748G flexlin LIN example

2,458件の閲覧回数
tonytony
Contributor I

I am using the S32 SDK with the SPC5748G devkit and I have setup the linflexd_uart_echo example which works but I really need to use this peripheral as a LIN peripheral, i.e. transmit header as master and receive slave response.

Does the SDK support configuration of this peripheral as linflexd_lin (as opposed to linflexd_uart)? I don't see it as a component within S32 IDE either.

Thanks

Tony

 

0 件の賞賛
返信
3 返答(返信)

2,448件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Tony,

this was already discussed here some time ago:

https://community.nxp.com/t5/S32-SDK/MPC57XX-EAR-SDK-LIN-Master-Slave-Example-Project/m-p/890681#M95...

and I'm afraid this has not been changed. There's no LIN support in the SDK for MPC5748G.

Regards,

Lukas

 

0 件の賞賛
返信

2,444件の閲覧回数
tonytony
Contributor I

Thanks Lukas

Can you confirm that the hardware supports LIN coms and it's just the SDK hasn't included it.  Or there is some bigger reason why the SDK team omitted such a basic peripheral demo application?

Many thanks for your support on these topics as I try get all the peripherals I need up and running.

Rgds

Tony

 

 

0 件の賞賛
返信

2,403件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Tony,

I'm sorry, I didn't get notification about new message due to some system issues. Probably too late but maybe for others: yes, LIN is supported by hardware, it's just not supported by SDK for some reasons. From reference manual: "The LINFlexD supports LIN protocol version 1.3, 2.0, 2.1 , and 2.2. "

Regards,

Lukas

 

0 件の賞賛
返信