S32DS Power Architecture SDK installation problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32DS Power Architecture SDK installation problem

跳至解决方案
2,246 次查看
0xEC
Contributor IV

Hi everyone,

I am using S32DS for generating project from scratch. I want to build project for mpc57xx evaluation board, so that I installed S32 SDK for Power Architecture. Installed package says

"The S32 Software Development Kit (S32 SDK) is an extensive suite of peripheral drivers, RTOS, stacks and middleware designed to simplify and accelerate application development on NXP MPC574x-B-C-G, MPC574x-P, MPC577xB-E-C, MPC574xR, S32R274, S32R264 and S32R372 Power Architecture based microcontrollers. "

but while I am trying to start new project and try to select MPC57xx processor, I could not find it. Has anyone face this same problem ? or are there any suggestions ?

Thank you,

0 项奖励
回复
1 解答
2,233 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi

you can follow below guide to create new project
https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-Project-MP...

Also you can create new one based on demo examples

PetrS_0-1654864198680.pngPetrS_0-1654864198680.png

BR, Petr

在原帖中查看解决方案

2 回复数
2,234 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi

you can follow below guide to create new project
https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-Project-MP...

Also you can create new one based on demo examples

PetrS_0-1654864198680.pngPetrS_0-1654864198680.png

BR, Petr

2,231 次查看
0xEC
Contributor IV

Thanks @PetrS  I will follow the tutorial.

0 项奖励
回复