S32DS Power Architecture SDK installation problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS Power Architecture SDK installation problem

Jump to solution
2,264 Views
0xEC
Contributor IV

Hi everyone,

I am using S32DS for generating project from scratch. I want to build project for mpc57xx evaluation board, so that I installed S32 SDK for Power Architecture. Installed package says

"The S32 Software Development Kit (S32 SDK) is an extensive suite of peripheral drivers, RTOS, stacks and middleware designed to simplify and accelerate application development on NXP MPC574x-B-C-G, MPC574x-P, MPC577xB-E-C, MPC574xR, S32R274, S32R264 and S32R372 Power Architecture based microcontrollers. "

but while I am trying to start new project and try to select MPC57xx processor, I could not find it. Has anyone face this same problem ? or are there any suggestions ?

Thank you,

0 Kudos
Reply
1 Solution
2,251 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi

you can follow below guide to create new project
https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-Project-MP...

Also you can create new one based on demo examples

PetrS_0-1654864198680.png

BR, Petr

View solution in original post

2 Replies
2,252 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi

you can follow below guide to create new project
https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-Project-MP...

Also you can create new one based on demo examples

PetrS_0-1654864198680.png

BR, Petr

2,249 Views
0xEC
Contributor IV

Thanks @PetrS  I will follow the tutorial.

0 Kudos
Reply