S32DS Power Architecture SDK installation problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS Power Architecture SDK installation problem

ソリューションへジャンプ
2,248件の閲覧回数
0xEC
Contributor IV

Hi everyone,

I am using S32DS for generating project from scratch. I want to build project for mpc57xx evaluation board, so that I installed S32 SDK for Power Architecture. Installed package says

"The S32 Software Development Kit (S32 SDK) is an extensive suite of peripheral drivers, RTOS, stacks and middleware designed to simplify and accelerate application development on NXP MPC574x-B-C-G, MPC574x-P, MPC577xB-E-C, MPC574xR, S32R274, S32R264 and S32R372 Power Architecture based microcontrollers. "

but while I am trying to start new project and try to select MPC57xx processor, I could not find it. Has anyone face this same problem ? or are there any suggestions ?

Thank you,

0 件の賞賛
返信
1 解決策
2,235件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi

you can follow below guide to create new project
https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-Project-MP...

Also you can create new one based on demo examples

PetrS_0-1654864198680.png

BR, Petr

元の投稿で解決策を見る

2 返答(返信)
2,236件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi

you can follow below guide to create new project
https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-Project-MP...

Also you can create new one based on demo examples

PetrS_0-1654864198680.png

BR, Petr

2,233件の閲覧回数
0xEC
Contributor IV

Thanks @PetrS  I will follow the tutorial.

0 件の賞賛
返信