Reprogram MPC5604E

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reprogram MPC5604E

2,056 Views
thiesteichmann
Contributor II

Hallo everyone,

 

i'd like to to reprogram the MPC5604E. So far i've downloaded the example software (Salsa Low Cost Reference Kit Aptina Camera version - demo SW + binaries). Now i'd like to analyse, edit and test the code. Unfortunately the example project is missing some folders (OS, Salsa). My question is: Is it possible to get these?

Any help would be greatly appreciated

Labels (1)
0 Kudos
Reply
2 Replies

1,794 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

if you want to modify the sample application, Freescale Autosar OS is needed. This note is copied from SalsaLowCostRefKitLibAPI.pdf:

"For evaluation purposes the sample application can be modified. In this case Freescale AUTOSAR OS/MPC560xE v.3.0 RTM should be installed into application\intapp_xxx\OS directory where scc subdirectory is expected."

Notice that it is commercial software, it is not provided for free:

Freescale AUTOSAR Software Solutions|Freescale

Regards,

Lukas

0 Kudos
Reply

1,794 Views
thiesteichmann
Contributor II

Hi,

we want to use the OS only for educational purposes at the Ostfalia -

University of Applied Sciences. Is it possible to get it for educational

purposes?

Redards,

Thies

Am 09.10.2015 um 09:00 schrieb lukaszadrapa:

>

Freescale Community

<http://jiveon.jivesoftware.com/mpss/c/fAA/PDcDAA/t.1r4/NW1cNm_gSvCqUQ9CiEx2dg/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQ-3D>

<http://jiveon.jivesoftware.com/mpss/c/fAA/PDcDAA/t.1r4/NW1cNm_gSvCqUQ9CiEx2dg/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQ-3D>

>

Reprogram MPC5604E

reply from Lukas Zadrapa

<http://jiveon.jivesoftware.com/mpss/c/fAA/PDcDAA/t.1r4/NW1cNm_gSvCqUQ9CiEx2dg/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQlPCh-2BdR0Iuh2b8GsySf-2BTzStW8Kcy62N7SZlPsQqm9PXJpFJHNa7nyleWxUK8Pkk-3D>

in /MPC5xxx/ - View the full discussion

<http://jiveon.jivesoftware.com/mpss/c/fAA/PDcDAA/t.1r4/NW1cNm_gSvCqUQ9CiEx2dg/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bRorSxS-2FfrSXtyorEQP4jO5nezm6ZWD5y-2FKZ8-2FwKcOI8rn6qX3JpWV904diHHmRMOg-3D>

>

0 Kudos
Reply