Reprogram MPC5604E

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Reprogram MPC5604E

2,102 次查看
thiesteichmann
Contributor II

Hallo everyone,

 

i'd like to to reprogram the MPC5604E. So far i've downloaded the example software (Salsa Low Cost Reference Kit Aptina Camera version - demo SW + binaries). Now i'd like to analyse, edit and test the code. Unfortunately the example project is missing some folders (OS, Salsa). My question is: Is it possible to get these?

Any help would be greatly appreciated

标签 (1)
标记 (2)
0 项奖励
回复
2 回复数

1,840 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

if you want to modify the sample application, Freescale Autosar OS is needed. This note is copied from SalsaLowCostRefKitLibAPI.pdf:

"For evaluation purposes the sample application can be modified. In this case Freescale AUTOSAR OS/MPC560xE v.3.0 RTM should be installed into application\intapp_xxx\OS directory where scc subdirectory is expected."

Notice that it is commercial software, it is not provided for free:

Freescale AUTOSAR Software Solutions|Freescale

Regards,

Lukas

0 项奖励
回复

1,840 次查看
thiesteichmann
Contributor II

Hi,

we want to use the OS only for educational purposes at the Ostfalia -

University of Applied Sciences. Is it possible to get it for educational

purposes?

Redards,

Thies

Am 09.10.2015 um 09:00 schrieb lukaszadrapa:

>

Freescale Community

<http://jiveon.jivesoftware.com/mpss/c/fAA/PDcDAA/t.1r4/NW1cNm_gSvCqUQ9CiEx2dg/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQ-3D>

<http://jiveon.jivesoftware.com/mpss/c/fAA/PDcDAA/t.1r4/NW1cNm_gSvCqUQ9CiEx2dg/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQ-3D>

>

Reprogram MPC5604E

reply from Lukas Zadrapa

<http://jiveon.jivesoftware.com/mpss/c/fAA/PDcDAA/t.1r4/NW1cNm_gSvCqUQ9CiEx2dg/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQlPCh-2BdR0Iuh2b8GsySf-2BTzStW8Kcy62N7SZlPsQqm9PXJpFJHNa7nyleWxUK8Pkk-3D>

in /MPC5xxx/ - View the full discussion

<http://jiveon.jivesoftware.com/mpss/c/fAA/PDcDAA/t.1r4/NW1cNm_gSvCqUQ9CiEx2dg/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bRorSxS-2FfrSXtyorEQP4jO5nezm6ZWD5y-2FKZ8-2FwKcOI8rn6qX3JpWV904diHHmRMOg-3D>

>

0 项奖励
回复