Reprogram MPC5604E

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reprogram MPC5604E

2,002件の閲覧回数
thiesteichmann
Contributor II

Hallo everyone,

 

i'd like to to reprogram the MPC5604E. So far i've downloaded the example software (Salsa Low Cost Reference Kit Aptina Camera version - demo SW + binaries). Now i'd like to analyse, edit and test the code. Unfortunately the example project is missing some folders (OS, Salsa). My question is: Is it possible to get these?

Any help would be greatly appreciated

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,740件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

if you want to modify the sample application, Freescale Autosar OS is needed. This note is copied from SalsaLowCostRefKitLibAPI.pdf:

"For evaluation purposes the sample application can be modified. In this case Freescale AUTOSAR OS/MPC560xE v.3.0 RTM should be installed into application\intapp_xxx\OS directory where scc subdirectory is expected."

Notice that it is commercial software, it is not provided for free:

Freescale AUTOSAR Software Solutions|Freescale

Regards,

Lukas

0 件の賞賛
返信

1,740件の閲覧回数
thiesteichmann
Contributor II

Hi,

we want to use the OS only for educational purposes at the Ostfalia -

University of Applied Sciences. Is it possible to get it for educational

purposes?

Redards,

Thies

Am 09.10.2015 um 09:00 schrieb lukaszadrapa:

>

Freescale Community

<http://jiveon.jivesoftware.com/mpss/c/fAA/PDcDAA/t.1r4/NW1cNm_gSvCqUQ9CiEx2dg/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQ-3D>

<http://jiveon.jivesoftware.com/mpss/c/fAA/PDcDAA/t.1r4/NW1cNm_gSvCqUQ9CiEx2dg/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQ-3D>

>

Reprogram MPC5604E

reply from Lukas Zadrapa

<http://jiveon.jivesoftware.com/mpss/c/fAA/PDcDAA/t.1r4/NW1cNm_gSvCqUQ9CiEx2dg/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQlPCh-2BdR0Iuh2b8GsySf-2BTzStW8Kcy62N7SZlPsQqm9PXJpFJHNa7nyleWxUK8Pkk-3D>

in /MPC5xxx/ - View the full discussion

<http://jiveon.jivesoftware.com/mpss/c/fAA/PDcDAA/t.1r4/NW1cNm_gSvCqUQ9CiEx2dg/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bRorSxS-2FfrSXtyorEQP4jO5nezm6ZWD5y-2FKZ8-2FwKcOI8rn6qX3JpWV904diHHmRMOg-3D>

>

0 件の賞賛
返信