Replacing MPC535 with MPC536

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Replacing MPC535 with MPC536

跳至解决方案
1,842 次查看
THensel
Contributor I

Hi,

we have an old product with uses the obsolete MPC535. We got a batch of electrically compatible MPC536 to use instead. I know it is also obsolete. My question is, are binaries for the MPC535 compatible to the MPC536. As I understand it, the only difference is that the MPC536 can use code compression but must not. So I hope that the default setting are the same for both controller so that the binaries don't have to be recompiled.

Thanks

T. Hensel

0 项奖励
回复
1 解答
1,829 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Torben,

yes, your binaries are compatible. The only difference is that MPC536 has code compression feature. The rest is exactly the same.

Regards,

Lukas

在原帖中查看解决方案

2 回复数
1,826 次查看
THensel
Contributor I

Thanks for the fast answer.

Best Regards,

Torben

0 项奖励
回复
1,830 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Torben,

yes, your binaries are compatible. The only difference is that MPC536 has code compression feature. The rest is exactly the same.

Regards,

Lukas