Replacing MPC535 with MPC536

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Replacing MPC535 with MPC536

Jump to solution
1,837 Views
THensel
Contributor I

Hi,

we have an old product with uses the obsolete MPC535. We got a batch of electrically compatible MPC536 to use instead. I know it is also obsolete. My question is, are binaries for the MPC535 compatible to the MPC536. As I understand it, the only difference is that the MPC536 can use code compression but must not. So I hope that the default setting are the same for both controller so that the binaries don't have to be recompiled.

Thanks

T. Hensel

0 Kudos
Reply
1 Solution
1,824 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Torben,

yes, your binaries are compatible. The only difference is that MPC536 has code compression feature. The rest is exactly the same.

Regards,

Lukas

View solution in original post

2 Replies
1,821 Views
THensel
Contributor I

Thanks for the fast answer.

Best Regards,

Torben

0 Kudos
Reply
1,825 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Torben,

yes, your binaries are compatible. The only difference is that MPC536 has code compression feature. The rest is exactly the same.

Regards,

Lukas