PWMMAC eTPU API inconsistent behavior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PWMMAC eTPU API inconsistent behavior

1,309件の閲覧回数
ukirde_pramod
Contributor I

We are using PWMMAC etpu library functions. We have observed the unclear behavior of this API.

Our assumptions based on application note (AN2969) is - 

When the duty cycle is configured in such a way that the On time of pulse is lower than half the dead time, the PWM turns off.

But our observations are different,

e.g.

When we try to give switching frequency of 20 Khz, dead time of 3.2 microseconds,  Duty cycle = 10% (5 microsecond),

we expect the pulse width of 1.8 microsecond, but we get 2.79 Microseconds.

we exercise this for different duty cycles but we didn't observe the consistency. 

Can you please explain this behavior?

ラベル(1)
0 件の賞賛
返信
1 返信

1,240件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, if it is still an issue, could you provide more details about your configuration? Thanks

0 件の賞賛
返信