Nested macro opening within "[!ERROR]

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Nested macro opening within "[!ERROR]

1,881 次查看
ma_cg
Contributor III

    Greetings,

       I previously responded in the comment section of my original question, but it seems that the technical support team might have missed it. Therefore, I am reposting my question here.

      When I configured devkit-mpc5748g using EB tresos27.1.0, MCAL, The corresponding MCAL links to  “https://nxp.flexnetoperations.com/control/frse/product?entitlementId=594560027&lineNum=1&authContact...

ma_cg_0-1723513433018.png

After the MCU module is configured, there is no problem in compiling. After the GPT module is added and configured, There came the "Parsing file "D:\EB tresos 27.1.0\EBtresosStudio_EBtresosStudio\plugins\Gpt_TS_T2D35M10I5R0/generate_PC/src/Gpt_Cfg.c (signed)", line "96"
[D:\EB tresos 27.1.0\EBtresosStudio_EBtresosStudio\plugins\Gpt_TS_T2D35M10I5R0/generate_PC/Gpt_VersionCheck_Src.m (signed):54]: Nested macro opening within
"[!ERROR]
"AUTOSAR release revision version number of the Basic Software Module Description ..." "

In this case, the message [!ERROR] does not close the loop correctly. Therefore, I modify the corresponding file as prompted, resulting in a signature problem. In summary, what I want to solve is the problem that [!ERROR] does not close the loop, and it is not necessary to modify the signature problem. 

I have exported my EB MCAL configuration project as an ARXML file and attached it here. Could you please help me debug it? #MPC5748   #NXP  DEVKIT-MPC5748G 

   Thank you for your suggesions!

 

标记 (1)
0 项奖励
回复
2 回复数

713 次查看
JwDouble
Contributor II

Hello,

I encountered the same problem as you, I want to ask how you solved it in the end,thanks!

0 项奖励
回复

1,849 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I have already replied in original post.

This to me looks like mismatch on your side and I was able to create with same plugins example code where is no issue present.

Therefore I asked you to export the full project. But I do not see any project in your demo.rar which I can use for generation test.

best regards,

Peter

0 项奖励
回复