MPC5777M GTM MCS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5777M GTM MCS

1,589 次查看
MuZhi
Contributor I

Hello, I am currently using MPC5777M GTM-MCS module, the GTM version is 104, and I want to get SDADC directly through MCS. Can this version support it?

标记 (1)
0 项奖励
回复
3 回复数

1,549 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Looking at our web I can see latest GMT config tool is: 1.1.0.0

petervlna_0-1743061295988.png

I expect that GTM config tool is for configuration of GTM module an not of an SDADC.

However I never tried it.

petervlna_1-1743061929355.png

Best regards,

Peter

 

 

0 项奖励
回复

1,537 次查看
MuZhi
Contributor I

Hello Peter,

I haven't used the configuration tool but am looking to implement this by writing code manually. Therefore, I would like to confirm whether the current GTM (GTM version V104) supports acquiring SDADC data directly through MCS.

Additionally, after downloading the GTM104 manual from the official website, I noticed that there are no multiplication or division instructions in the MCS instruction set. Could you please confirm if this is due to the current architecture not supporting these operations or if it's an incompleteness in the manual? If possible, could you share a complete version of the manual?

1514905266_0-1743425749755.png

 

Best regards,

MuZhi

0 项奖励
回复

1,501 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

You can download the from following link:

https://community.nxp.com/t5/MPC5xxx/Generic-Timer-Module-104-reference-Manual/m-p/466367

Could you please confirm if this is due to the current architecture not supporting these operations

In the time the GTM was released it was not needed so those are not supported.

NXP is not using GTM anymore, we prefer eTPU which is also on new devices.

I would like to confirm whether the current GTM (GTM version V104) supports acquiring SDADC data directly through MCS.

I do not see any direct connection from ADC to GTM. Nor any triggers to GTM.

I assume you will have to use DMA for automated data transfer and also some trigger.

petervlna_0-1743578157354.png

Best regards,

Peter

 

 

0 项奖励
回复