Need TRK-MPC5604B CAN interface help

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need TRK-MPC5604B CAN interface help

ソリューションへジャンプ
4,541件の閲覧回数
jkm89
Contributor II

Which jumpers must be connected to activate the SBC? Do I need external power?

ラベル(1)
0 件の賞賛
返信
1 解決策
4,232件の閲覧回数
jkm89
Contributor II

Solved it: J1 needed to be connected 5-6.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,233件の閲覧回数
jkm89
Contributor II

Solved it: J1 needed to be connected 5-6.

0 件の賞賛
返信
4,232件の閲覧回数
olivierkieffer
Contributor II

And the CAN is working now? How do you check it?

I've attached a PEAK-USB interface and I always get a BUSHEAVY message ...

THE EVB is clearly terminated and I've put a 120Ohm resistor on the PEAK side.

0 件の賞賛
返信
4,232件の閲覧回数
olivierkieffer
Contributor II

I'm struggling myself with the CAN on a TRK-MPC5634 board. What I figured out so far, is that I need an external power supply (9-12V) and that the MC33903 needs to be set in DBG mode with a jumper (J5). Still I get nothing on the DB9 (CAN-H and CAN-L remain to 0V)

0 件の賞賛
返信
4,232件の閲覧回数
jkm89
Contributor II

I emailed tech support about this issue and they said J5 needs to be installed and J4 needs to be removed (debug mode). Also, whenever I set the switch to the "on" position, the SBC starts getting very hot, which is concerning me.

0 件の賞賛
返信