Missing Symbol Definitions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Missing Symbol Definitions

3,111件の閲覧回数
fixed-term_juli
Contributor I

I use the 3-Phase PMSM Motor Control Development Kit with Qorivva MPC5604P MCU and the User interface of NXP you can see ins Screen.PNG.

If I start the program, there is a failure -Missing symbol Definitions- you can see at Variables.PNG.

But it is connected with the board. (Communication.PNG)

Where is the problem and how can I fix it?

(The motor runs if I use the switch up/down or I update the target with the User interface. But there is no change if I vary the input variables)

0 件の賞賛
返信
1 返信

3,025件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Did you follow quick start guide and compiled and loaded the code to micro?

Do you have correctly set Freemaster files?

regards,
Peter

0 件の賞賛
返信